Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
VPM-Slide16

There are several ways the normally closed thermal breakers can be used. The thermal switch could be connected to the control circuit that turns the transformer on and off, or a simple relay circuit could be used. On this slide an example schematic for a circuit with a relay that could be used for the VPM240-15600 is shown.

PTM Veröffentlicht am: