Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
440 DMM-Scope Slide 11

Shown here is the set-up for measuring resistance. Turn the selector dial to the resistance position and connect the test leads to the input jacks. Be sure the circuit being tested is turned OFF. Touch the test leads to the device under test. The resistance is displayed in the digital display.  Also, to check the continuity of a circuit follow the same steps for resistance but press the F2 button. This converts the Resistance function into a Continuity Tester. Touch the test leads to the device under test. Continuity is indicated by an audible beep and resistance is displayed in the digital display.

PTM Veröffentlicht am: