Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
LED Driver Overview Slide 3

In choosing an LED Driver, the first step is to determine whether a constant-current or constant-voltage power source is required in an application. The designer must also identify the maximum wattage load the driver will encounter and then choose a driver rated for slightly higher. Other factors include dimming capabilities, efficiency, size, safety, warranty, and so on.

PTM Veröffentlicht am: