Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
RF Introduction to TMS37157 PaLFI Slide 8

The Battery Charge command is used to power the connected microcontroller without a battery. This command can also be used to charge an attached system battery. When a Battery Charge command has been received, the TMS37157 applies a voltage of 3.4V to the VBAT pin. The charge current depends mainly on the antenna of the LC tank circuit and the field strength of the base station.

PTM Veröffentlicht am: