Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
TPS75005 Integrated Solution for C2000 MCUs Slide 2

The TPS75005 is compatible with several C2000 controllers including the Delfino family. A unique feature of this solution is that not only does it power the C2000, it also has the correct power down sequence that is needed for the C2000 controller. This is a totally integrated solution which means external supervisors are not required.

PTM Veröffentlicht am: