Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
LM5017 100 V 600 mA Synchronous Buck Converter Slide 14

As mentioned earlier in the presentation, the LM5017 has an under-voltage lockout pin. It does not have an over-voltage function, which could be a reasonably popular request. The circuit shown on this slide is a design to implement an OVP using a small number of external components.

PTM Veröffentlicht am: