Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Capacitive Touch Sensing Slide 10

Using the configurations already provided in the structure.c file, the API TI_CAPT_RAW is used to measure the sensors. Since F as a function of C is being measured, when the user touches the wheel or button, it increases capacitance and therefore lowers the frequency. In this demo, it is demonstrated that with Code Composer Studio, the user is able to graph the representation of the frequency with time, as well as see the raw data, shown by the two arrows.

PTM Veröffentlicht am: