Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Product List
Heat Shrink Micro-Molded Slide 3

The features and benefits of the micro molded heat shrink product line are highlighted in this slide.  They are much smaller in size than TE Connectivity's other molded parts. The image shows a regular size 202F211 with several of the micro boots. The boots come in an expanded form with the option of an adhesive lining matching the material of the boot. The boots are currently offered  as standard parts in -25  polymeric elastomer , -100  low halogen, and -12  flexible fluoroelastomer as standard, but can be made in virtually all of the various TE Connectivity material choices . Micro boots provide environmental sealing  and  protection against  mechanical abuse at the cable-to-connector interface.

PTM Veröffentlicht am: