Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
LED 15
The TS19820CS has built in PWM or linear dimming, DCM mode PFC built in and the ability to drive an external MOSFET. No optocoupler is required in the circuit implementation and the device has ample protection modes built in. Integrating a 3.3 V regulator provides the ability to power a microcontroller or other digital circuitry along with powering the IC itself. This offers the designer reduced parts count and savings on space and cost as well as design and assembly time.
PTM Veröffentlicht am: