Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
reliability demo
As previously mentioned, Swissbit conducts a number of qualification tests. These include reliability tests with a high number of samples and tests under extreme temperature conditions as well as functional compatibility and compliance tests. These tests even include testing until the device goes end of life. Another group of tests are the environmental and stress tests, such as the previously mentioned temperature cycle test. These qualification tests prove the design and production stability. Additionally, Swissbit tests each individual drive at specified temperatures to continuously monitor the quality of the production process.
PTM Veröffentlicht am: