Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Power Inductor Basics Slide 8

The right hand rule is an easy way to determine and recall the direction of the magnetic field lines using the known conventional current direction. Because of the orientation (shown by the right hand rule) of the magnetic field produced by the changing current, it is extremely advantageous to wind the conductor into a coil shape. The theoretical inductance formula on the next slide will help to illustrate the relationship between the number of turns in a coil and the resulting inductance.

PTM Veröffentlicht am: