Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
sllimm positioning

Which IPM should be used for the application? The nominal power of the motor will be the easiest parameter to consider when selecting a module. The SLLIMM™-nano products will cover electric motors up to 300 W. The higher power will require the use of a SLLIMM-nano 2nd series. SLLIMM™ modules will be used up to 3 kW. Please always remember that additional data is required to find the right module for a specific application: switching frequency, current level, voltage level, and what control algorithm will be used can drastically change the performances of a module. SLLIMM™ modules are available in two different packages: full molded (FM) or Direct Bond Copper (DBC). The DBC option will provide a lower thermal resistance, thus improving the performances of the module at higher power. The FM option represents the best trade-off between cost and performances for medium power motors.

PTM Veröffentlicht am: