Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Gate Drivers Overview Slide 8

The SmartDRIVE name comes from the features added to the standard half-bridge gate driver, such as the smart shutdown that works in conjunction with the fault comparator, the fault comparator, the operational amplifier optimized for field oriented control in a BLDC motor, and programmable dead time and interlocking features which are integrated in the L6390.

PTM Veröffentlicht am: