Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
wireless-gecko-slide4

Wireless Gecko is more than an IC. It is a platform for building solutions. From the IC standpoint it provides a foundation with a ARM Cortex M4 and integrated 2.4GHz multiprotocol transceiver that is capable of providing up to +19.5 dBm output power. It integrates key IP around low power such as integrated DC/DC, hardware crypto and low energy peripherals. In fact, the device has a complete and robust set of peripherals designers would expect to find on a full featured MCU. Of course it is a lot more than that, it is also about how users get their products to market. Silicon Labs have focused on enabling designers with the fastest time to market by having a complete set of tools and software. Silicon Labs provides certified software stacks for ZigBee/Thread and Bluetooth Smart as well as proprietary software for low cost options where designers do not need to tie into existing eco-systems. Additionally, they provide reference designs for RF optimization, as well as specific applications such as lighting and of course modules for fast time to market and reduced development cost. Finally, Silicon Labs' award winning Simplicity Studio ties this all together by providing a single location for all user needs through evaluation, prototyping, development and even optimization. Wireless Gecko truly is a complete platform to build a product around.

PTM Veröffentlicht am:
PTM Updated on: 2017-06-16