Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Streamline-Slide5

For upgraded impact protection and a stylish appearance, a décor seal can be provided in yellow, red, blue, green, and graphite grey colors. The décor seal is constructed of TPE rubber and allows the handheld device to be deployed with an ingress protection of IP65. Battery compartments can be integrated into the Streamline with gaskets to ensure that the electronics are protected from external moisture. Battery compartments can be provided for use with 3 AAA, 3 AA or, 4 AA batteries, depending upon the size of the selected enclosure.

PTM Veröffentlicht am: