Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Image of ROHM H-Bridge Drivers for DC Brush Motors - High-Performance Startup

Typically, the highest current will flow when turning on the motor (start-up current). ROHM’s H-Bridge driver has current limit function that can be externally configured to the lowest possible value while still allowing the motor to start up to prevent any reliability issues by high inrush current. Also, it is possible to work permanently in current limiting mode to enable a constant current (or constant motor torque) operation. Current limit is set by external reference voltage VREFx and current detection resistor RNFx.

PTM Veröffentlicht am:
PTM Updated on: 2021-02-25