Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Application Example

Shown here is a high level application example where the BD39040MUF-C has been added between the existing PMIC and system processor. The BD39040MUF-C supports multiple channels up to four power good signals, a watchdog timer, timing clock, reset monitoring, and self-test type features. Along with power, all the communication commands sent from the processor to the PMIC are verified, tested, and diagnosed as needed.

PTM Veröffentlicht am: