Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Accelerometer-Slide8

Non-linearity is a measure of how much a device output differs from the ideal behavior over the full sensor range and is measured as a percentage of maximum deviation to full scale.  It is important to know how non-linear a device is so that one can account for and reduce error in the overall system. Kionix accelerometers have low non-linearity at less than 1% of full scale.

PTM Veröffentlicht am: