Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Develop with RL78/G24

Discover how to develop RL78/G24 using the various tools for each step. First, if the customer is not sure which MCU is suitable for the project, use the Web Simulator. No evaluation board or software tools are required, and the customer can quickly check the MCU performance using only a web browser. After verifying the performance, an evaluation board will be helpful. Then, the customer can use a debugger and programmer with tools such as E2/E2 Lite and Bridge IC. Finally, Renesas also provides a PG-FP6 Flash programmer and manufacturing tools. As for software tools, Renesas has compilers, IDEs, and development support tools, including familiar partners as well as Renesas’ in-house tools.

PTM Veröffentlicht am: