Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Great Coverage

RIIM™ has a long range of up to 700 m in urban environments and up to 20 km line of sight (LOS) with the High Power module and up to 200 m in urban areas and 5 km LOS with a regular module. The RIIM protocol supports up to 29 hops, given a small payload. This means that the RIIM network can cover an area of up to 40 x 40 km squared. It is also important to note that the network is 2-way symmetric to also send data to the sensors or control units.

PTM Veröffentlicht am: