Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Image of PANJIT Bridge Rectifier Introduction - M4 Series

The M4 surface-mount bridges are designed with gull wing outline to ensure better solderability. The TRR of M4 bridges is <250 ns for EMI improvement. The IF range from 2A to 4A which is the maximum IF within the same packaging measurement range in the industry.

PTM Veröffentlicht am: