Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
corner wiring
How does Corner Wiring Duct save space? Shown on this slide is a top view of how the application is done today. In this case two 3 x 4 channels are used, ran vertically. They are moved out from the corner to allow access to remove covers. Their panel surface also does not run into the corner. Corner Wiring Duct can fit tight into the corner of the enclosure and replace the two channels with one to save mounting space in existing enclosures on both the side and back panel.
PTM Veröffentlicht am: