Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Solid foundation
It is important to note that a network design starts with a logical framework that shows the connections required between devices to ensure viable exchange of information between networked devices. The logical framework is important but the customer will find that a physical network design is equally important because it highlights the distances between the connected devices and the media that is to be used with the required connectivity end-points, bonding and grounding points. The physical design quickly points to the need to aggregate the connection points into distribution nodes (Distributors - as shown in the TIA 1005A star topology) and the cabling sub-systems needed. Two possible cabling sub-systems choices are used in the architecture; Fiber cables for all horizontal runs (normally over 100 meters in length) and copper for all vertical runs, within work cells, and all connections to the Edge points and devices.
PTM Veröffentlicht am: