Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Industrial SD Slide 3
Panasonic’s Industrial SD mission is to bridge the gap between NAND flash memory and industrial requirements. NAND flash memory die shrink is inevitable to achieve larger capacity and lower cost but reliability and performance degrades accordingly. As industrial requirements are becoming more severe, Panasonic industrial SD bridges this gap by adopting industrial NAND flash memory, reducing error rates and enhancing performance by Panasonic designed controller. As more than 80% of NAND flash failure cannot be reproduced, Panasonic industrial SD focuses on preventing failure outflow by carrying out 100% screening test before shipment.
PTM Veröffentlicht am: