Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Electro + Chemistry

Instead of having a pair of reactions (a reduction and an oxidation) with the corresponding chemical agents, electronics replace one of the agents delivering or accepting electrons. For example, by applying an anodic potential at an iron surface, the formation of rust is provoked. Instead of the oxygen which accepts the iron’s electrons in nature, the device applying the anodic potential accepts the electrons. This electronic is used to make chemical reactions happen and study them.

PTM Veröffentlicht am: