Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
SRAM Overview and Applications Slide 8

This table shows the advantages and disadvantages of each memory type. If the memory has to be written often and quickly, then Serial SRAM will provide a better solution then EEPROM. In addition, serial SRAM provides a more cost effective and low-power solution than FRAM. Lastly, Serial SRAM has a much lower pin count, smaller footprint, and lower cost than Parallel SRAM. However, when it comes to selecting which memory product to use, designers must understand the application needs.

PTM Veröffentlicht am: