Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slide10

One of the first questions an engineer will ask when initially investigating the possibility of moving to MOSFET technologies is in regards to the signal integrity. MOSFET’s inherently will display a clipping, or delay, in the rise time of the signal. Two of the key performance characteristics of a MOSFET relay are the off-state capacitance (Coff) and on-state resistance (Ron). Due to the reactive elements in a MOSFET capacitance, when combined with other elements prevent instantaneous changes in voltage from occurring.  This rising edge of the wave form will appear more “rounded” when a MOSFET is used. To reduce the effects of a rounded leading edge, Omron has several families of MOSFET relays specifically designed for applications that require a low off-state capacitance and on-resistance combination or “CxR”.

PTM Veröffentlicht am: