Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PPLC-Slide6

There are a variety of housing models available for the ODU MINI-SNAP® Series L with IP50 and IP68 rating. Ratings are possible in reference to the end device and also in unmated form. A visual red dot indicates the 12 o’clock position. Both front and rear panel mounted receptacles are available.

PTM Veröffentlicht am: