Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
esd sensitive
In this example, we have a customer application that requires ESD protection to 25 kV (Kilovolts). An IC to be used in this application only has internal protection rated at 4kV. The gap between the IC’s internal protection of 4kV and the customer’s application (25kV) can be closed with ESD Diodes.
PTM Veröffentlicht am: