Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
NXS Concept

The NXS topology is similar to that of the LSF in that it uses a pass transistor but also adds internal one-shot circuits to accelerate the rising edge of signals through the device. In addition, the pull-up resistors, which were external for the LSF family, are now internal. When using the NXS family, the OE pin should be connected to VCC(A) and the higher voltage domain should be connected to the B-side.

PTM Veröffentlicht am: