Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
MoSys Supplied FPGA RTL

Shown here is the support that is available from Peraso for easy adoption of the Peraso devices in a direct way to reduce the latency of the design effort and support a quicker time to market. First, in this regard, Peraso can support the development of the controller that resides in the FPGA; it is even possible to have Peraso provide one that already exists, or at a minimum, an example controller can be provided that can be the basis off of which a custom design can be developed. Secondly, in addition to the controller, Peraso can provide RTL that implements the GCI protocol which is used as the protocol for the SerDes links. This is code that has been used on dozens of designs and has been field-tested for over a decade. Finally, the third area in which Peraso can support the quick adoption of the accelerator engines into a design is the devices themselves. Peraso has been supplying the devices to customers for over a decade with hundreds of thousands of devices in the field.

PTM Veröffentlicht am: