Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
MIC23-Slide6

HyperLight Load™ Step-Down Regulators are also very cost-effective solutions capable of displacing traditional fixed frequency PWM step-down devices in many cases. In situations where constant switching frequency is required, HyperLight Load regulators can emulate a fixed frequency switching regulator by simply increasing the value of inductor placed at the output. In the case of the MIC23031, use of a 4.7µH inductor results in a constant 4MHz switching frequency from a 10mA output current all the way up to the maximum rating of 400mA.

PTM Veröffentlicht am: