Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
LCD-Slide9

There are many advantages in utilizing LCD display technology versus other display technologies, such as VFD (Vacuum Fluorescent Display). LCDs are more aesthetically pleasing, as they can display almost any design and the sleekness of LCDs provides many space-saving advantages. They are also very light and are therefore more portable. The user-interface with an LCD is far superior when compared to VFD technology. Also, LCDs are typically more cost-effective, not to mention more ecologically-friendly when it comes to power consumption. An average LCD’s power consumption is in the area of 30 micro-watts when compared to an average VFD display, which can be significantly higher.

PTM Veröffentlicht am: