Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Design-Slide12

As one considers the bandwidth requirements of Ethernet, it has continued to increase as one progresses from 10 Base-T to 100 Base-T to 1000 Base-T to 10GbE. As this bandwidth increases, any additional loading on the wire pairs can reduce rate and reach capabilities of the Ethernet interface. A parallel capacitance or a common mode capacitance can cause impedance mismatches and distort the signaling eye to the point of causing data loss. Therefore, placing surge protection across the line or in a common mode arrangement, the designer must consider the impedance of the line. At higher frequency bands, this off-state capacitance of any surge protector must be sufficiently low so as not to cause signal distortion.

PTM Veröffentlicht am: