Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide7

A transient is a very narrow disturbance on the normally steady voltage bus. If there is an MOV protection device installed between the line and ground, the disturbance will cause a current to flow in the MOV and the overvoltage condition will be drastically reduced. The excess energy will get dissipated as heat inside the MOV before it has a chance to move into sensitive circuitry downstream.

PTM Veröffentlicht am: