Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
LT8300-Slide4

The slide shows the internal positioning of the LT8300. The LT8300 closely compares to the LT3511, with the differences being that the LT8300 has a lower quiescent current and is in a smaller package. The LT3511 on the other hand has output voltage temperature compensation, a bias voltage input capability, and adjustable feedback loop compensation parts. The LT3512 is another part in this family and is almost identical to the LT3511 except it has a higher power switch rating.

PTM Veröffentlicht am: