Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
HO Series of Mid Range Current Transducers Slide 5

The HO is an ASIC based transducer. This ASIC contains all the electronics in the transducer including the hall cell. The HO is a galvanically isolated device capable of measuring AC or DC current. It has an Over Current Detection (OCD) pin that makes it unique. The HO is available in three mounting styles, PCB mount with integral bus bar, PCB mount with aperture and panel mount with aperture.

PTM Veröffentlicht am: