Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
ConnexLink-Slide10

Test results are shown in the View RX Packets window. Successfully received packets will be shown in a black text, error packets will be in red. The two types of errors are Data Timeouts or Data Errors. Data Errors could be caused by an incorrect baud rate on the port, if the radios are too close and are saturating or other interferers. Data timeouts can be caused by saturation, but are usually due to an incorrect setting or an incorrect setup. The Test Results will display the total number of error packets and provide an estimated bits per second.

PTM Veröffentlicht am: