Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
switch open
The second and primary method is by the MLCC absorbing the charge of the ESD source. This method can be modeled by a simple schematic showing a charged capacitor discharging into another capacitor through a switch. When the switch is open, the two capacitors are not electrically connected and have no influence on one another. When voltage is applied to capacitor “C1”, it will have a charge “Q1” which is the product of the Capacitance “C1” and Voltage “V1”.
PTM Veröffentlicht am: