Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
MX44 Series Slide 9

In summary, JAE’s MX44 Series is a Waterproof Board-to-Cable Connector that has a compact design with waterproof contacts and structure. With a tight sealing rubber in the mating area, it enables a compact design and improves vibration resistance. The box type contact is strong against external forces and the contact area has a double spring which is resistant to twisting. Contacts are set in position by inserting the retainer from the wire side which protects the lock part of the connector.

PTM Veröffentlicht am: