Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
JL10-Slide4

The JL10 series has a low-profile compact design that adopts a one-touch bayonet locking method for mating. The JL10 receptacle is a single-touch and screw mating dual type: one-touch mating when using the JL10 plug and screw mating when using the MIL-standard MS connector, etc. The angle type cable leaders can be set in eight arbitrary directions by 45° increments. The JL10 series cable clamp is the same cable clamp as the JL04V, it is also a UL and TUV approved product.

PTM Veröffentlicht am: