Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Slide8

The ISL9238 uses the same buck-boost operation with the four switching FETs, an inductor, and a battery connecting FET. However, it can operate in reverse boost and buck-boost mode as well to deliver power out of the USB port for charging an external electronic device. With the ISL9238, Renesas added a new “autonomous charging and end of charge feature” that allows the user to charge the battery without waking up the system. This device is pin-to-pin compatible with the ISL9237, and the EC code is also compatible if the new feature is not used.

PTM Veröffentlicht am: