Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
demo kit
Honeywell offers a demonstration kit for evaluation of the Integrated Pressure Transducer (IPT). The Honeywell IPT Demo Board firmware implements a set of commands to send the pressure and temperature output from the IPT over an RS-232 communication line. In addition, EEPROM read/write commands are supported to change select contents of the IPT EEPROM. SPI signals are brought to the edge of the demo board allowing the user to examine communication between the demo board microcontroller and the IPT. The demonstration kit includes an evaluation board, an RS-232 communication cable, an AC adapter, Microsoft Windows software, and a user’s manual. The demonstration kit is intended to be used in a laboratory desktop environment and can be ordered by adding the suffix “–A” to the end of any IPT model number.
PTM Veröffentlicht am: