Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Features (cont'd) 1

The crimped contacts are simply pushed into the female connector housing from the rear and will click into place with a retaining tang. To remove the contact from the housing, a special tool or a standard precision flat-bladed screwdriver can be inserted into the highlighted window near the front face of the connector. This folds the retaining tang inwards and the contact can now be pulled out from the back of the housing.

PTM Veröffentlicht am: