Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Associated Content
Other Physical Features

All the best features from the Gecko-SL series are retained on the Gecko-MT: Back-potting walls to contain added epoxy resin, for additional strain relief. Position number one identifier on the signal pins (see the Component Specification for full pin numbering). Finally, three polarization features to assist easy mating without the possibility of error.

PTM Veröffentlicht am: