Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List Associated Content
Horizontal Male Backshell – PCB Mount

Horizontal male backshells are available as single items and can be used with horizontal PCB mounted male connectors with Through-board or Surface Mount terminations. When used with a ground plane in the PCB, the connector will be fully shielded. The backshell can be assembled at any time after the connector is mounted to the board.

PTM Veröffentlicht am: