Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Image of HARTING RJ Industrial® MultiFeature Series - Features Continued 1

The highlight of the RJ45 series are the integrated blades, which shorten the individual strands to the correct length when closing the connector. It is essentially a built-in side cutter. This eliminates this time-consuming work step, and the assembly is more than 25% faster. There is no longer a need to shorten the individual wires eight times using the wire cutter and the quality of the connection process is also improved.

PTM Veröffentlicht am: