Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
XRP7714-slide19

The synchronization function that is used is actually synchronizing the system clock frequency, so technically synchronizing the two system clocks together designers could program one part at say 300kHz and another one at 600kHz.

PTM Veröffentlicht am: