Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
EM Microelectronics Bluetooth® Beacons - In Development

EM is currently working on two new beacon products. The first is called “Tiny Beacon” which will be EM’s smallest unit. It is intended to be less obtrusive for people to wear on a wrist strap, and is also designed to be used for asset tracking with small packages. It will be waterproof, and it will have a push button and an LED. Instead of using a removable battery, it will operate on a small coin cell with a two-week life, using an environmentally-friendly technology suitable for disposal. EM is also working on a rugged dual-mode beacon that will come in two options: one with BLE® and UHF/RFID for asset tracking and security, and the other with BLE and NFC for secure pairing with mobile devices. EM is working on new features like enhanced security with Bluetooth®, and also cloud connectivity.

PTM Veröffentlicht am: