Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
electroswitch-slide10

Electrical specifications include current carrying capacity, current rating and voltage rating. Current carrying capacity, measured in amps, is the maximum load that a switch will carry when the contacts are in a closed position. Current and voltage ratings are the tested amperage and voltage capacity when switching contact positions under load. An electrical arc occurs when switching between positions under load which over a period of time will cause contact wear. A switch with the contacts closed has no arc, and the carrying capacity is higher.

PTM Veröffentlicht am: